I2C interface with MPC5200

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2C interface with MPC5200

913 次查看
ashwinibhat
Contributor II

Please provide flow to work I2C interface on MPC5200

标签 (1)
3 回复数

804 次查看
Pavel
NXP Employee
NXP Employee

Look at attached file. It is simple I2C program example for the MPC5200B board. It is CodeWarrior project for the Lite5200B board.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

804 次查看
ashwinibhat
Contributor II

Thanks Pavel.

I will refer this source code.

0 项奖励
回复

803 次查看
ashwinibhat
Contributor II

Can anybody tell answer of this question?

0 项奖励
回复