I2C interface with MPC5200

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C interface with MPC5200

909件の閲覧回数
ashwinibhat
Contributor II

Please provide flow to work I2C interface on MPC5200

ラベル(1)
3 返答(返信)

800件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at attached file. It is simple I2C program example for the MPC5200B board. It is CodeWarrior project for the Lite5200B board.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

800件の閲覧回数
ashwinibhat
Contributor II

Thanks Pavel.

I will refer this source code.

0 件の賞賛
返信

799件の閲覧回数
ashwinibhat
Contributor II

Can anybody tell answer of this question?

0 件の賞賛
返信