I had tried to modified the demo (MPC5674F)to MPC5644A , but it always meet the problem that the program loop in the function (void FlashConfig(void)) which is in the file( _ppc_eabi_init.c ).
Waiting for help,
Thanks.
Hi,
my recommendation is - do not modify original project. Create new project for MPC5644A and then import the drivers and update main.c file.
There are chip specific initializations which are different - size of SRAM for initialization, flash wait states... It's much easier to start with new empty project.
Regards,
Lukas
Hello Lukas,
Thank you very much. I do created the new project for MPC5644A. Question is I don't konw how to import the drivers and update main.c. I tried for several times, then program cannot go to main(), just stay in the function I mentioned above. So, could you please show me how to import and update?
Sincerely,
L.W