How to use CAN to send multiple sets of data at once

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use CAN to send multiple sets of data at once

Jump to solution
1,532 Views
yinlei
Contributor III

If I have 32 sets of data, how to use the CAN, once the data sent out   。

  NOW  I want to send 8 bytes of dataThere are 32 sets of such dataSo call the  function  (Transmit_Message_1) 32 times。BUT  ’I think it's too long to wait;A lot of time wasted in this statement(while (CAN_0.MB[1].CS.B.CODE != 0x8););So now, I would like to put 32 data in different BUFFER inside。Such as MB [0] -MB [31],And then send the data together。My purpose is to reduce the sending function to send the completion time, in order to allow the processor to do other things.My leader told me that the data inside the MB is very fast, the time is mainly wasted here(while (CAN_0.MB[1].CS.B.CODE != 0x8);)So how can i improve this code?I can solve this problem from which part of the reference manual。

Tags (1)
1 Solution
1,280 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

from my point of view, it is not necessary to wait until the message is sent from message buffer. Use for example FOR loop. In the FOR loop, fill MB0 and set code to 0xC, fill MB1 and set code to 0xC and so on.

To check, if MB was successfully transmitted, you can use for example interrupt. Another way is check message buffer status as soon as you will fill it again. The method you use is strictly dependent on your application requirements.

Regards,

Martin

View solution in original post

5 Replies
1,280 Views
oloooloo
Contributor III

1. If You want to use only one MB, it is necesser to wait until end of sending. But the way You implemented is passive waiting. Use active waiting, means dont go in to loop but let the code go and check BUSY flag activelly.

2. better slution is to use more then one MBs, just fill one after another and mark to send same time.

1,280 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I am not sure if I understand your question correct. Could you please clarify your requirement? Which microcontroller you use?

Regards,

Martin

1,280 Views
yinlei
Contributor III

 hi, Martin Kovar; 

  the  MCU  is  MPC5775K;

  NOW  I want to send 8 bytes of dataThere are 32 sets of such dataSo call the  function  (Transmit_Message_1) 32 times。BUT  ’I think it's too long to wait;A lot of time wasted in this statement(while (CAN_0.MB[1].CS.B.CODE != 0x8););So now, I would like to put 32 data in different BUFFER inside。Such as MB [0] -MB [31],And then send the data together。My purpose is to reduce the sending function to send the completion time, in order to allow the processor to do other things.My leader told me that the data inside the MB is very fast, the time is mainly wasted here(while (CAN_0.MB[1].CS.B.CODE != 0x8);)So how can i improve this code?I can solve this problem from which part of the reference manual。

  void Transmit_Message_1(uint32_t* buf)
{
CAN_0.MB[1].CS.B.CODE = 0x8; //MB TX inactive
CAN_0.MB[1].ID.B.ID_STD = 0; //set message STD ID
CAN_0.MB[1].DATA.W[0] = *buf; //data0 set
CAN_0.MB[1].DATA.W[1] = *(buf + 1); //data1 set
CAN_0.MB[1].CS.B.DLC = 8; //message length 8 bytes
CAN_0.MB[1].CS.B.RTR = 0; //remote frame disable
CAN_0.MB[1].CS.B.IDE = 0; //extended bit disable
CAN_0.MB[1].CS.B.SRR = 0; //not used with STD_ID
CAN_0.MB[1].CS.B.CODE = 0xC; //MB once transmit data
while (CAN_0.MB[1].CS.B.CODE != 0x8);
}

       thank  you  very much !

0 Kudos
Reply
1,281 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

from my point of view, it is not necessary to wait until the message is sent from message buffer. Use for example FOR loop. In the FOR loop, fill MB0 and set code to 0xC, fill MB1 and set code to 0xC and so on.

To check, if MB was successfully transmitted, you can use for example interrupt. Another way is check message buffer status as soon as you will fill it again. The method you use is strictly dependent on your application requirements.

Regards,

Martin

1,280 Views
yinlei
Contributor III

thank you very much

0 Kudos
Reply