How to upload multiple elf to MPC5674F?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to upload multiple elf to MPC5674F?

504件の閲覧回数
chunghohwang
Contributor II

Hi~~

Our project should divide the following executable files(elf) for certification:
- one of elf performs the function of the bootloader.
- one of elf performs the main functions.
- one of elf stores data into external memory.

I have encountered the following problems during developing the project using Code Warrior.

1. I will upload two or more executable files to one target board. How do i modify the supplied lcf file and startup code (MPC5674F based).

2. I use the ICDPPCNEXUS debugger included our code warrior package. I want to upload multi executable files to the target board using the this debugger. when i use this debugger, it seems that the previously uploaded elf file is deleted.

3. I want to jump from the A project to the start point of B project. How do i use assembler? Thank you for your example. (The bl command was executed but i was failed)

0 件の賞賛
返信
0 返答(返信)