I need to send 8 bytes command at a time, as the Correct.PNG.
But the SPI_PUSHR can only send 2 bytes TXDATD at a time, and after the SPI_PUSHR sent the TXDATD, the MOSI will be pulled high, as the Incorrect.PNG.
Is there a way to solve the problem of MOSI pull high?
Thanks!
Dear Peter:
Thank you for your reply!
But the document only refers to the control of PCS, I have finished this part.
In the reference manual, the SOUT is also pulled high between the two transfers.
Is there a way let SOUT pulled low between the two transfers?
Thanks!
B.R.
Don