How to correctly configure CAN Rx Mailboxes Mask Register in MPC5748G?
I want to receive message with specific ID .For instance 0x000,0x111,0x222 and so on.
As follows:
It seems that the mask highest bit is not in effect.
0 - 400:
0000 0000 0000
0100 0000 0000
44 - 444:
0000 0100 0100
0100 0100 0100
111 - 511:
0001 0001 0001
0101 0001 0001
Because of the RX FIFO,it is right that to configure the CAN_RXFGMASK as 0x1fffffff. [0:28]
However there are some mistakes in somewhere.
Then I force CAN_RXFGMASK to be configured as 0x3fffffff. It does work.
Is there some mistakes in my knowledge?
where is mistake?Please inform me in detail .
regards.
已解决! 转到解答。
Hi,
mask within a RXFGMASK should be shifted left by 1 bit as you can see in chapter 43.4.17 of the RM
so, to have exact match you need to set RXFGMASK = 0x3FF80000 (assuming standard ID is received).
Most probably the driver function does not shift the value properly.
With the RXFGMASK = 0x1FFC0000 the MSB of the ID is don't care, that's the reason you received such IDs.
BR, Petr
Hi,
mask within a RXFGMASK should be shifted left by 1 bit as you can see in chapter 43.4.17 of the RM
so, to have exact match you need to set RXFGMASK = 0x3FF80000 (assuming standard ID is received).
Most probably the driver function does not shift the value properly.
With the RXFGMASK = 0x1FFC0000 the MSB of the ID is don't care, that's the reason you received such IDs.
BR, Petr
Thank you for your reply.
Yes,you are right.
There may be a bug in the SDK.
The API(settting Rx FIFO global mask) dose not deal with CAN_MCR[IDAM] .
It only checks either standard id or extended id,but it is useless for CAN_RXFGMASK.
And it will clear the bits form 31 to 29. So it is never correct that use the API(FLEXCAN_DRV_SetRxFifoGlobalMask) to configure the CAN_RXFGMASK.
Best regards,gao
Hello, Mr. Gao,
@泽乾 高
Could you share the code you showed?
I just want to know how to use RxFIFO to receive CAN MSG with multiple CAN IDs. I am using the API(status_t FLEXCAN_DRV_ConfigRxMb) to receive CAN MSG now ,but it can only receive the msg which CAN ID was defined.
Many Thanks~
You can configure the mask as follows:
FLEXCAN_DRV_SetRxMbGlobalMask(instance, FLEXCAN_MSG_ID_STD, 0x0U);
(void)FLEXCAN_DRV_SetRxIndividualMask(instance, FLEXCAN_MSG_ID_STD, Individual_num, 0x0U);
Hope it works for you.
Regards.