FreeRTOS- like OS for MPC5634M on CW Classic IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS- like OS for MPC5634M on CW Classic IDE

1,119 Views
arjunraveendran
Contributor III

I am working on MPC5634M platform on Code warrior 2.7 Classic IDE. I know there is no ready made support from FreeRTOS for this chip. 

Could anyone suggest an alternate RTOS which supports this chip that i can port for my application?

Thanks in advance.

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

878 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

AUTOSAR OS is for sure supporting MPC5634M.

You can also use ARC CORE.

ARCCORE - AUTOSAR Products 

For more details you have to ask ARCORE as this is not NXP product.

Peter

878 Views
arjunraveendran
Contributor III

Hello,

Thanks for the reply. Currently, I am not looking for a commercial licensed solution.

Could you point towards any free/open source options.

Thank you.

0 Kudos
Reply

878 Views
jfrey
Contributor IV

ChibiOS has worked on e200 cores in the past.

The developer works for STMicro.  The topic has been brought up to support the newer NXP chips now that there is a free compiler available.

878 Views
arjunraveendran
Contributor III

Thanks a lot for the answer.

I will check the compatibility with ChibiOS .

0 Kudos
Reply