Flexray communication between channel A and channel B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexray communication between channel A and channel B

1,663件の閲覧回数
qingsong_wu
Contributor I

I was told that a Flexray controller has 2 channel, channel A and channel B. Assume that I connect a Flexray node A channel A with another Flexray Node B channel B, if the communication can be established between node A and B?

(Involved mcu is mpc5748g).#communication flexray

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,435件の閲覧回数
truongtran1
Contributor II

If my memory is good, the flexray frame consist of header CRC checksums, the header CRC and Frame CRC. The header CRC is the same and the Frame CRC is different on channel A and B, you can refer to the Flexray specification. Thus,  you cannot technically do the communication from node A send out a frame on channel A and node B receive that frame on channel B.

0 件の賞賛
返信

1,435件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm not Flexray expert but channel A and channel B can work independently (various network topology can be used) to increase bandwidth. For safety critical applications, messages can be transmitted simultaneously on both channels in order to achieve a redundancy.

Regards,

Lukas

0 件の賞賛
返信