Flexray communication between channel A and channel B

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flexray communication between channel A and channel B

1,661 次查看
qingsong_wu
Contributor I

I was told that a Flexray controller has 2 channel, channel A and channel B. Assume that I connect a Flexray node A channel A with another Flexray Node B channel B, if the communication can be established between node A and B?

(Involved mcu is mpc5748g).#communication flexray

标记 (1)
0 项奖励
回复
2 回复数

1,433 次查看
truongtran1
Contributor II

If my memory is good, the flexray frame consist of header CRC checksums, the header CRC and Frame CRC. The header CRC is the same and the Frame CRC is different on channel A and B, you can refer to the Flexray specification. Thus,  you cannot technically do the communication from node A send out a frame on channel A and node B receive that frame on channel B.

0 项奖励
回复

1,433 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm not Flexray expert but channel A and channel B can work independently (various network topology can be used) to increase bandwidth. For safety critical applications, messages can be transmitted simultaneously on both channels in order to achieve a redundancy.

Regards,

Lukas

0 项奖励
回复