Flexray communication between channel A and channel B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexray communication between channel A and channel B

1,659 Views
qingsong_wu
Contributor I

I was told that a Flexray controller has 2 channel, channel A and channel B. Assume that I connect a Flexray node A channel A with another Flexray Node B channel B, if the communication can be established between node A and B?

(Involved mcu is mpc5748g).#communication flexray

Tags (1)
0 Kudos
Reply
2 Replies

1,431 Views
truongtran1
Contributor II

If my memory is good, the flexray frame consist of header CRC checksums, the header CRC and Frame CRC. The header CRC is the same and the Frame CRC is different on channel A and B, you can refer to the Flexray specification. Thus,  you cannot technically do the communication from node A send out a frame on channel A and node B receive that frame on channel B.

0 Kudos
Reply

1,431 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm not Flexray expert but channel A and channel B can work independently (various network topology can be used) to increase bandwidth. For safety critical applications, messages can be transmitted simultaneously on both channels in order to achieve a redundancy.

Regards,

Lukas

0 Kudos
Reply