Hi, I m using MPC5674F for Flexray application.
I want to know the cycle counter when the core starts Flexray communication after being normal active.
I expected that cycle counter is 0 for all nodes within flexray network. But it was not 0 and different.
Thank you.
Thank you for quick Reply, Petr.
Our Flexray Parameters are as follows.
- Communication Cycle is 500 us / 5 ms.
- 2 Nodes are in Flexray Cluster (3 nodes will be joined later)
- 3 Static slots (Using Key slot) / Only Dynamic Slots are using for Data Exchange.
I have three questions here.
1. Do all nodes coupled to Flexray communication use the same Cycle Counter?
2. If 1 is correct, how will Flexray communication be affected if the Cycle Counter between nodes is different?
3. When node 1 sends data to Cycle 10, Slot 1, when does node 2 actually receive data?
Is it Cycle 10 or 11?
Thank you