Hello,
Flash erase is not working for me with the MPC5777M.
I am using an example from MPC5748G-Flash_RW-SSD_GHS614 that I found on the forums. None of the following steps fail with an error and pFlashCheckStatus is returning with C55_DONE. However, it does not erase anything. I am trying to erase memory sector 0x09640000.
This is my code:
#define C55_REG_BASE 0xFFFE0000
#define MAIN_ARRAY_BASE 0x00404000
#define UTEST_ARRAY_BASE 0x00400000
#define C55_PROGRAMMABLE_SIZE 0x80
SSD_CONFIG ssdConfig = {
C55_REG_BASE, /* C55 control register base */
MAIN_ARRAY_BASE, /* base of main array */
{ 0, 0, 0 }, /* blocks info of low address space */
{ 0, 0, 0 }, /* blocks info of mid address space */
{ 0, 0, 0 }, /* blocks info of high address space */
0, /* number of blocks in 256K address space */
UTEST_ARRAY_BASE, /* base of UTEST array */
TRUE, /* interface flag indicate main or alternate interface */
C55_PROGRAMMABLE_SIZE,/* programmable size */
FALSE /* debug mode selection */
};
void func()
{
uint32_t returnCode = 0; /* Return code from each SSD function. */
uint32_t result = 0;
uint32_t lowBlockSelect, midBlockSelect, highBlockSelect;
CONTEXT_DATA CtxData;
N256K_BLOCK_SEL n256KBlockSelect;
// Flash Init
returnCode = pFlashInit(&ssdConfig);
if (C55_OK != returnCode)
{
return;
}
returnCode = pSetLock(&ssdConfig, C55_BLOCK_256K_FIRST, 0xFDFFFFFF);
if (C55_OK != returnCode)
{
return;
}
//erase the mid block
lowBlockSelect = 0x00000000;
midBlockSelect = 0x00000000;
highBlockSelect = 0x00000000;
n256KBlockSelect.first256KBlockSelect = 0x02000000;
n256KBlockSelect.second256KBlockSelect = 0x00000000;
returnCode = pFlashErase(&ssdConfig,
C55_ERASE_MAIN,
lowBlockSelect,
midBlockSelect,
highBlockSelect,
n256KBlockSelect);
if (C55_OK != returnCode)
{
return;
}
while(1)
{
returnCode = pFlashCheckStatus(&ssdConfig, C55_MODE_OP_ERASE,&result, &CtxData);
if(returnCode != C55_INPROGRESS)
{
break;
}
}
}
I have also done it in the following way after searching for information on the forums with similar results:
C55FMC.LOCK2.R = 0b11111101111111111111111111111111;
C55FMC.MCR.B.ERS = 1;
C55FMC.SEL2.R = 0b00000010000000000000000000000000;
*(unsigned int*)0x09640000 = 0xFFFFFFFF; //interlock write
C55FMC.MCR.B.EHV = 1;
while(C55FMC.MCR.B.DONE == 0);
C55FMC.MCR.B.EHV = 0;
C55FMC.MCR.B.ERS = 0;
Do you have enabled cache? If so, it is possible you have incoherent data between cache and target memory. In other words flash block is erased but you read data already pre-fetched in the cache.
So you can either disable cache before flash erasing/programming or invalidate cache after erasing/programming.