Example code on the implementation of Flexray on DEVKIT-MPC5748G

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example code on the implementation of Flexray on DEVKIT-MPC5748G

1,407 次查看
christos_patrin
Contributor I

Hello dear members,

I recently purchased the DEVKIT-MPC5748G and I wanted to ask if it's possible to get an example code for a very simple task; reading one message via flexray. I have searched through the various examples of the S32 Design Studio but I haven't found anything quite useful for this task. If this is not possible, any recommendations on where to start from for the software development of this task would be appreciated.

I am currently reading the reference manual of the MPC but it would be ideal for me if I could accelerate my work and the understanding on how to achieve this task through some examples.

Thank you for your time in advance.

3 回复数

1,108 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

another way is use FlexRay driver from Vector, but remember, this driver is under license.

Regards,

Martin

0 项奖励
回复

1,108 次查看
petervlna
NXP TechSupport
NXP TechSupport

Yes, thats true.

But MCAL nor vector drives are not example codes. They are full drivers certified for automotive.

I don't think they can serve as example codes at all.

The flexRAY protocol is so complicated then it is easiest to just use existing drivers instead of writing your own. (dynamic configuration, etc...)

Peter

0 项奖励
回复

1,108 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I had a talk with FlexRAY expert.

According to him, our customers use only Autosar MCAL flexray drivers.

Unfortunately, there is no simple example of FlexRAY available.

regards,

Peter

0 项奖励
回复