I am having issue getting the CAN Example for the MPC5746R to work? I am using the 57XX mother board with the MPC5746R-252DS. I would expect that this example would just work.
I have verified that the pin jumpers J37 and J38 are in the 2-3 position. I have also tried with them in the 1-2 position.
I am using s32DS 2017.R1 and an iSystems debugger.
Hi Ron,
I found and solved this problem.
When using your configuration
MAXMB in this register is not set to 0x3F successfully, it is 0xF. Because of that "This field can be
written only in Freeze mode because it is blocked by hardware in other modes". Only 16 MBs can be used in this case.
So I add that "CAN_1.MCR.B.MAXMB = 63;". Now , 64 MBs can be used. it's fine.
Hello Ron,
the example you use is created in S32 Design Studio v1.1 and unfortunately, it cannot be import and compiled in S32DS 2017.R1, because there were some significant changes in compiler.
I recommend you create new project in S32DS 2017.R1 and manually copy all necessary source code into new project.
Regards,
Martin
Martin,
I did not have any issues compiling the example. Example compiles and runs on the hardware, but I don't see any activity on the CAN bus. I did create a new project in 2017.R1 and copied over the the code from the FlexCAN project, but I still don't see any CAN Activity.