ERROR BFD:

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERROR BFD:

704件の閲覧回数
dineshs
Contributor I

BFD: D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5: section .sbss lma 0x40009a18 adjusted to 0x4000ec18

BFD: D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5: section .bss lma 0x40009a2c adjusted to 0x4000ec2c

BFD: D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5: section .interp lma 0x4000ec18 adjusted to 0x400124d0

BFD: D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5: section .dynsym lma 0x4000ec2c adjusted to 0x400124e1

BFD: D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5: section .dynstr lma 0x4000ec2c adjusted to 0x400124e1

BFD: D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5: section .hash lma 0x4000ec3c adjusted to 0x400124ef

BFD: D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5: section `.data' can't be allocated in segment 3

LOAD: .sbss .data .dynamic

BFD: D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5: The first section in the PT_DYNAMIC segment is not the .dynamic section

C:/DDC-I/usr/local/cross-compilers/gcc-4.6.1/bin/powerpc-motorola-elf-objcopy:D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5[.text]: Bad value

BFD: D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5: section `.data' can't be allocated in segment 3

LOAD: .sbss .data .dynamic

BFD: D:/GSSW/GSS/output/powerpc-motorola-elf/diagnostic/stSTc4t5: The first section in the PT_DYNAMIC segment is not the .dynamic section

 

 

 

getting errors in open arbor environment with mpc5676r microcontroller..............

ラベル(1)
0 件の賞賛
1 返信

549件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

please DO NOT DUPLICATE thread at community.

I have already posted you an answer at this thread:

how to migrate from codewarrior to DDC-I OpenArbor 

Regards,

Martin

0 件の賞賛