Driver for KSZ8081RNACA - PHY in MPC5748G Devkit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Driver for KSZ8081RNACA - PHY in MPC5748G Devkit

883 次查看
sandeepvl
Contributor III

Hi all, 

I am trying to run a web server in MPC5748G Devkit. For this, I need a TCP/IP stack for which I have selected lwIP. I am yet to select the RTOS to be used. Considered candidates are FreeRTOS and eCOS.

lwIP can run on bare metal without having any operating system. I got an lwIP package ported for MPC5748G EVB from this community - MPC5748G ENET . It works perfectly in EVB and I can run an http webserver on it successfully.

Now I have to take this to Devkit. The relevant difference between the EVB and Devkit are:

1. EVB supports MII (by default) and Devkit supports only RMII.

2. EVB has dp83848c as the phy controller whereas Devkit has KSZ8081RNACA as the phy.

The ported lwIP package has the driver for dp83848c. I need the driver for KSZ8081RNACA.

Does anybody have this driver? Has anyone tried to execute lwIP in Devkit?

Thanks

Sandeep

0 项奖励
回复
1 回复

561 次查看
martin_kovar
NXP Employee
NXP Employee

Hello Sandeep,

unfortunately, we do not have driver for KSZ8081RNACA. Maybe you will be luck and someone will provide you this driver.

Another possibility is to port lwIP driver for KSZ8081RNACA, but I do not know, how difficult it is.

Regards,

Martin

0 项奖励
回复