Does anybody managed CAN networking with TRK-MPC6534M EVB?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does anybody managed CAN networking with TRK-MPC6534M EVB?

跳至解决方案
1,396 次查看
olivierkieffer
Contributor II

Hello,

 

I can't get CAN to work. The board has a MPC5634m + SBC 33903 for CAN communication.

I've powered the board with 12V, supply source is is to SBC, SBC is in DBG mode, there is 5V on 5V-CAN pin of the SBS.

The board is terminated (60-Split-60) and I connected an PEAK CAN-USB on the other side that I terminated as well with 120Ohm.

 

I've used the sample application from the cookbook (100kb/s) for the MCU, but the ESR register is indicating BUS OFF.

This is working in loopback mode.

 

The only signal I see on the CAN_A_Tx pin is the atteched one (blue trace), which I think correspond to BUS ERROR recovery, isn't it?

 

Thanks for your help.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,238 次查看
olivierkieffer
Contributor II

Freescale Tech support solved it. The SBC needs to be configured via SPI to turn the transceiver on (even in debug mode).

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,239 次查看
olivierkieffer
Contributor II

Freescale Tech support solved it. The SBC needs to be configured via SPI to turn the transceiver on (even in debug mode).

0 项奖励
回复