Difference between MPC5748G Non-HSM and HSM PN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between MPC5748G Non-HSM and HSM PN

508 Views
hongpingxu-b364
NXP Employee
NXP Employee

Hi,

 

My customer will enable security feature based on their mature project. Only the SPC5748GMMJ6 ()N78S, Trace Code: 2244) has been changed to SC667691MMJ6 (0N78S, Trace Code: 1906).

Customer reported that the Machine Check exception generates at SPI[5] initialization when the HSM is enabled. The MSCR is 0008A008,.and MCAR is 0xFBFA4030.

Another puzzling problem on HSM board is that the CAN frames are not transmitted properly although written to message buffers. After online debugging, we found that the data did not correctly write the target buffer, but the offset buffer.

According to the above issue, we had push customer to:

1.) Configure PRAMCx_PRCR1[FT_DIS] to 1 before the PLL enable mode is switched.

2.) Check the Clock distribution with “AN5392” excel tool.

3.) Errata items.

 

Regarding Difference between Non-HSM and HSM PN, could you please help us to clarify this question? Eg.:

1.) Memory occupation

2.) How much working current will be increased for HSM module.

3.) HSM firmware for SC667691MMJ6 (0N78S, Trace Code: 1906)

4.) Other Special sequence if have.

 

 

Best regards,

 

Hornby

0 Kudos
Reply
3 Replies

488 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @hongpingxu-b364 

could you create a ticket for this, so we can assign it to AE?

https://support.nxp.com/s/?language=en_US

Thanks,

Lukas

0 Kudos
Reply

437 Views
hongpingxu-b364
NXP Employee
NXP Employee

Hi,

 

Created.

Case: 00597929 (nxp.com)

 

Best regards,

Hornby

 

0 Kudos
Reply

433 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Thanks, I reassigned it to AE.

0 Kudos
Reply