Dear Mr. Mrs.
I use MPC5777C. When I try to delete data and write data on block0 64 kb (0x00000000 - 0x0000FFFF). I don't face with error. But When I try to programming empty block0 256 kb flash block (0x00800000-0x0083FFFF). My controller cause IVOR 1 exception. I couldn't find reason of this situation.
解決済! 解決策の投稿を見る。
Hi,
it looks like problem related to Read-While-Write (RWW) error.
RWW is supported only between partitions. That means we are not allowed to access a partition which is being erased or programmed. If we access such partition, it leads to bus error.
Your code must be executed from another partition or from RAM memory and interrupt handlers should not read the partition as well.
To find more details about the partitions, see Table 4-2 in the reference manual:
https://www.nxp.com/webapp/Download?colCode=MPC5777CRM
Regards,
Lukas
Hi,
it looks like problem related to Read-While-Write (RWW) error.
RWW is supported only between partitions. That means we are not allowed to access a partition which is being erased or programmed. If we access such partition, it leads to bus error.
Your code must be executed from another partition or from RAM memory and interrupt handlers should not read the partition as well.
To find more details about the partitions, see Table 4-2 in the reference manual:
https://www.nxp.com/webapp/Download?colCode=MPC5777CRM
Regards,
Lukas