Hi,
I am using S32 Design Studio.
S32 Design Studio for Power Architecture
Version: 1.2
Build id: 170613
(c) Copyright Freescale Semiconductor 2016. All rights reserved.
(c) Copyright NXP 2017.
MCU == MPC5777C
evb == MPC5777C EVB
debugger == Multilink universal fx
Operating System == Win7x64,Win8x64 Case 1: System clock : 192 MHz(PLL0) DSPI module Clock : 96 MHz PER CLK SELECT : PLL0 PER CLK : 96 MHz SCK BAUD RATE : 4 MHz In this case the Data send on MOSI line is received properly on MISO line.Case 2: System clock : 264 MHz(PLL1)In both the case SCK baud rate is same which is derived from PER CLK but module clock is different. Is DSPI module clock has any effect on data send and receive functionality?DSPI module Clock : 132 MHz
PER CLK SELECT : PLL0 PER CLK : 96 MHz SCK BAUD RATE : 4 MHz In this case the Data send on MOSI line is not received properly on MISO line.
Hi David,
As per your suggestion i have changed the DSPI module clock to 66 MHz which is less than maximum 100 MHz frequency.
But still the problem remain same and i am not able to receive the data properly.
Thanks and Regards,
Sourabh
Hi David,
here is system clock initialization of core clock 264 MHz.
System clock : 264 MHz(PLL1)
DSPI module Clock : 66 MHz
void SystemClk_init(void)
{
PLLDIG.PLL0CR.B.CLKCFG = 0; // Disable PLL0
PLLDIG.PLL1CR.B.CLKCFG = 0; // Disable PLL1
SIU.SYSDIV.B.PLL0SEL= 0x0; // PLLOSEL = 0 The crystal oscillator (XOSC) is the clock source for PLL0
SIU.SYSDIV.B.PLL1SEL = 0x1; // PLL1SEL = 1 The PHI1 output of PLL0 is the clock source for PLL1
// configure PLL0 to 192 MHz (40 MHz XOSC reference)
//configure PLL1 to 264 MHz (48 MHz PLL0 PHI1 output reference)
/* Configure PLL0 Dividers - 160MHz from 20Mhz XTAL oscillator */
PLLDIG.PLL0DV.B.RFDPHI1 = 0x0C;
PLLDIG.PLL0DV.B.RFDPHI = 0x3;
PLLDIG.PLL0DV.B.PREDIV = 0x5;
PLLDIG.PLL0DV.B.MFD = 0x48;
/* Wait for stable XOSC */
SIU.RSR.B.XOSC = 0x1; //0 XOSC clock not stable yet
//1 XOSC clock is stable
/*Turn on PLL0 and wait for lock */
PLLDIG.PLL0CR.B.CLKCFG = 0x3; //Turn on PLL0
while(1)
{
if(PLLDIG.PLL0SR.B.LOCK == 0x01) // PLL is locked
break;
}
/* Configure PLL1 Dividers - 200MHz from 20Mhz XTAL oscillator */
PLLDIG.PLL1DV.B.RFDPHI = 0x02;
PLLDIG.PLL1DV.B.MFD = 0x16;
/*Turn on PLL1 and wait for lock */
PLLDIG.PLL1CR.B.CLKCFG = 0x3; //Turn on PLL0
while(1)
{
if(PLLDIG.PLL1SR.B.LOCK == 0x1) // PLL is locked
break;
}
/* Select clock dividers and sources */
SIU.SYSDIV.B.LCK = 0x0; // LCK = 0 SIU_SYSDIV register is unlocked and writes are permitted
SIU.SYSDIV.B.PLL0SEL= 0x0; // PLLOSEL = 0 The crystal oscillator (XOSC) is the clock source for PLL0
SIU.SYSDIV.B.PLL1SEL = 0x1; // PLL1SEL = 1 The PHI1 output of PLL0 is the clock source for PLL1
SIU.SYSDIV.B.PERCLKSEL = 0x1; // PERCLKSEL = 1 Clock is connected to the non-FM clock domain
SIU.SYSDIV.B.PERDIV = 0x0; // PERDIV = 0 Divide by 2.
SIU.SYSDIV.B.MCANSEL = 0x0; // MCANSEL = 0 The crystal oscillator (XOSC) is the clock source for the MCAN modules.
SIU.SYSDIV.B.SYSCLKSEL = 0x2; // SYSCLKSEL = 11 The system clock is driven by the non FM PLL (PLL0)
SIU.SYSDIV.B.FMPERDIV = 0x1;
SIU.SYSDIV.B.ETPUDIV = 0x1; // ETPUDIV = 1 Divide by 1.
SIU.SYSDIV.B.SYSCLKDIV = 0x4; // SYSCLKDIV = 100 Divide by 1
SIU.SYSDIV.B.PCSEN = 0x0; // PCSEN = 0 PCS disabled
SIU.ECCR.R =0x00000581;
SIU.SDCLKCFG.R = 0x0000000B;
SIU.LFCLKCFG.R = 0x00000001;
SIU.PSCLKCFG.R = 0x000100BF;
}
Whether you have seen following clock calculator. You may configure your clock settings by clicks and it checkes all frequency limits. In the summary tab, you may see configuration of all registers.
https://www.nxp.com/docs/en/application-note/AN12176.pdf
https://www.nxp.com/docs/en/application-note-software/AN12176SW.zip
Hope it helps.
Hi David,
I have checked the application note AN12176 which you have mention.
In that application note i have found out MPC5777C Frequency limits here snap is attached.
Here
FM_PER_CLK = 132 MHz (MAX) which drive the module clock of DSPI.
PER_CLK = 132 MHz (MAX) which drive Protocol clock of DSPI.
So right now i am using PER_CLK 96 MHz through which i derived SCK baud rate 4 MHz.
Case 1: System clock : 192 MHz(PLL0) DSPI module Clock : 96 MHz PER CLK SELECT : PLL0 PER CLK : 96 MHz SCK BAUD RATE : 4 MHz In this case the Data send on MOSI line is received properly on MISO line.Case 2: System clock : 264 MHz(PLL1)DSPI module Clock : 132 MHz
PER CLK SELECT : PLL0 PER CLK : 96 MHz SCK BAUD RATE : 4 MHz In this case the Data send on MOSI line is not received properly on MISO line.
I have only changes the DSPI module clock which FM_PER_CLK from initially 96 MHz to 132 MHz and in this case my DSPI not working properly.
Why is this happening ?