DEVKIT-MPC5744P CAN Connections

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DEVKIT-MPC5744P CAN Connections

974 次查看
mlg556
Contributor I

I'm having trouble with making the physical connections for CAN communication on the DEVKIT-MPC5744P board. Let's say CAN Bus 0 is transmitting and CAN Bus 1 is receiving a message. I have set CAN Bus 0 Receive Pin to B1 and Transmit to B0. Similarly CAN Bus 1 has A15 for receive and A14 for transmit. Which jumper connections should I make to enable data transfer between these two modules ? Where should I connect the CAN0H and CAN0L pins ? I don't see any high or low pins for CAN1, only receive and transmit.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

780 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

I checked MPC5744P devkit and unfortunately, it is not possible to interconnect two CAN modules, because there is only one CAN transceiver.

Also, CAN0 pins are not routed to external connector, so it is not possible to connect it with CAN1 pins. Only possibility is interconnect two boards together.

Sorry for any inconvenience.

Regards,

Martin

0 项奖励
回复