Current license does not allow downloading C++ code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Current license does not allow downloading C++ code

1,624件の閲覧回数
enes
Contributor II

Hi,

I m developing a small C project for MPC5674f and i m taking the error on the topic although i didnt use any C++ file on my project.  I m using Code Warrior Basic. There is no problem with building the project but when i click the debug button i m teking the error. I have attached a screen clip. 

Installed Products:
- CodeWarrior for MCU
Version: 10.6

Thanks for helping...

0 件の賞賛
5 返答(返信)

1,313件の閲覧回数
enes
Contributor II

Update:

I tried to debug it on RAM and it worked.

0 件の賞賛

1,313件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please share your project? From my point of view, this error is false positive and there is another problem with the project, but I need to check your project on my side.

Do you have some license for CW10.6 or you use evaluation version?

Regards,

Martin

0 件の賞賛

1,313件の閲覧回数
harshithanagari
Contributor I

Hi Martin,

I have the same issue. I initially installed Evaluation version and then updated the license file after purchasing the Standard annual license.

Thanks,

Harshitha

0 件の賞賛

1,313件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello Harshitha,

as I wrote in the previous post, I have never seen this error on my side and I need some example project which demonstrates the issue. I am not able to reproduce it on my side by my own.

Could you please share some example project with me?

Regards,

Martin

0 件の賞賛

1,313件の閲覧回数
enes
Contributor II

Yes i m using server licance for CW basic adition 10.6.

i m sorry, it is forbidden to send any content of the project to anywhere via network in my company. Thanks for helping Martin...

0 件の賞賛