Clock configuration for LIN module with MPC5777M EVM Board ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock configuration for LIN module with MPC5777M EVM Board ?

644 Views
anishchoudhary
Contributor III

I am working with MPC5777M  EVM board for LIN module implement. I did clock configuration as following but I am not able to establish the connection between two LIN port over the LIN bus. Please find the following clock configuration and make me sure I am on right trace or not ? If  not then please tell me what changes i will do to establish communication between two LIN port over the LIN bus ?

void system160mhz(void){
    {
        MC_CGM.AC3_SC.B.SELCTL = 0x01u;            //connect XOSC to the PLL0 input
        MC_CGM.AC4_SC.B.SELCTL = 0x01u;            //connect XOSC to the PLL1 input

        // Set PLL0 to 300 MHz with 40MHz XOSC reference
        PLLDIG.PLL0DV.R = 0x4002100Fu;                 // PREDIV =  1, MFD = 15, RFDPHI = 2, RFDPHI1 = 8

        MC_ME.RUN_MC[0].R = 0x00130070u;            // RUN0 cfg: IRCON,OSC0ON,PLL0ON,syclk=IRC

        // Mode Transition to enter RUN0 mode:
        MC_ME.MCTL.R = 0x40005AF0u;                    // Enter RUN0 Mode & Key
        MC_ME.MCTL.R = 0x4000A50Fu;                    // Enter RUN0 Mode & Inverted Key
        while (MC_ME.GS.B.S_MTRANS) {};                // Wait for mode transition to complete
        while(MC_ME.GS.B.S_CURRENT_MODE != 4u) {};    // Verify RUN0 is the current mode

        // Set PLL1 to 600 MHz with 40MHz XOSC reference
        PLLDIG.PLL1DV.R = 0x0001001E;                 // MFD = 30, RFDPHI = 1

        MC_ME.RUN_PC[0].R = 0x000000FE;                // enable peripherals run in all modes
        MC_ME.RUN_MC[0].R = 0x001300F4;                // RUN0 cfg: IRCON, OSC0ON, PLL1ON, syclk=PLL1

        MC_CGM.SC_DIV_RC.R = 0x00000001;              //! System clock divider ratios will change with next update.  Not required for Cut 1.
        MC_CGM.DIV_UPD_TYPE.R = 0x80000000;          //! System clock divider ratios updated on writing MC_CGM.DIV_UPD_TRIG.  Not required for Cut 1.

        MC_CGM.SC_DC2.R = 0x800B0000;                // PBRIDGEA/PBRIDGEB_CLK at syst clk div by 12 ... (50 MHz)
        MC_CGM.SC_DC1.R = 0x80050000;                // SXBAR_CLK at syst clk div by 6 ... (100 MHz)
        MC_CGM.SC_DC0.R = 0x80020000;               // FXBAR_CLK, BD_CLK, IOP_CLK at syst clk div by 3 ... (200 MHz)
        MC_CGM.SC_DC3.R = 0x80010000;                // COMP/CHKR_CLK at syst clk div by 2 ... (300 MHz)
        MC_CGM.SC_DC4.R = 0x800A0000;                // CLKOUT at syst clk div by 11 ... (54.55 MHz)

        MC_CGM.DIV_UPD_TRIG.R = 0xfeedface;         //! System clock divider ratio updates triggered.  Not required for Cut 1.
        while (MC_CGM.DIV_UPD_STAT.B.SYS_UPD_STAT == 1) //! Wait for System Clock Divider Update Status == 0. Not required for Cut 1.
        {
            // wait only
        }

        // Mode Transition to enter RUN0 mode:
        MC_ME.MCTL.R = 0x40005AF0;                    // Enter RUN0 Mode & Key
        MC_ME.MCTL.R = 0x4000A50F;                    // Enter RUN0 Mode & Inverted Key
        while (MC_ME.GS.B.S_MTRANS == 1u )
        {
            // Wait for mode transition to complete
        }
        while(MC_ME.GS.B.S_CURRENT_MODE != 4)
        {
             // Verify RUN0 is the current mode
        }

        MC_CGM.AC0_SC.R = 0x02000000;            // Select PLL0 for auxiliary clock 0
        MC_CGM.AC0_DC0.R = 0x80050000;        // PER_CLK : Enable aux clk 0 div by 6 … (50 MHz)
        MC_CGM.AC0_DC4.R = 0x80020000;            // Enable auxiliary clocks for LIN_CLK : 0 div by 3 … (100 MHz)
      //  MC_ME.PCTL15.R = 0x00000000u;             // Enable SIUL2 clock
        //MC_ME.PCTL92.R = 0x00000000u;         // Enable SIUL2 clock for LINFlexD_0.
        //MC_ME.PCTL92.R = 0x00000000u;         // Enable SIUL2 clock for LINFlexD_0.
    }
}

Tags (1)
1 Reply

494 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I see no issue with this clock setting.

BR, Petr