Clock Select for UART of MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock Select for UART of MPC5744P

1,684 Views
hbw
Contributor I

Hi,I am debugging the UART function of the MPC5744P using the Evaluation Board.But,I find a problem :

 When I begin to send the data ,the program will stop at 

                                                       while (LINFlexD_0.UARTSR.B.DTFTFF == 0);

I think it may duo to the reason that I select the wrong clock for it.Who can explain this problem for me.

Thanks,Best Wishes.

0 Kudos
5 Replies

1,177 Views
mikailaltintas
Contributor III

Hi,

Thank you HB W for answer. I found solution. Problem is about clearing DRFRFE flag.

In ISR I use  

LINFLEX[0]->UARTSR.B.DRFRFE = 1;

to clear flag. When I use this also DTFTFF flag clearing. So 

while (LINFlexD_0.UARTSR.B.DTFTFF == 0); is locked.

We have to use 

LINFlexD_0.UARTSR.R &= 0x00000004;

to clear DRFRFE flag. 

I think this is important so I will creat new topic and write all to there.

0 Kudos

1,177 Views
mikailaltintas
Contributor III

Hi, I have similar problem but my problem is not about clock. If there is no data on receive I can send data but if data received when I send data  ,the program will stop at 

                                                       while (LINFlexD_0.UARTSR.B.DTFTFF == 0);

I put a secureCounter to while loop so it is go on working but I want to know why this happens. If I increase baud rate I see that event occurrence decrease. So I think that uart is not work full dublex.  Manual Reference says Uart is Full duplex but it is working as half dublex. 

My configuration is listed below:

nbLINFlex = 0;

LINFLEX[nbLINFlex]->LINCR1.B.INIT = 1; // enter initialization mode


LINFLEX[nbLINFlex]->UARTCR.B.UART = 1; //0=LIN 1=UART
LINFLEX[nbLINFlex]->UARTCR.B.PCE = 0; //0 = parity disabled, 1 = parity enabled
LINFLEX[nbLINFlex]->UARTCR.B.PC0 = 0; //0 = even parity, 1 = odd parity
LINFLEX[nbLINFlex]->UARTCR.B.WL0 = 1; //0 7-bit data + parity bit *** 1 8-bit data (or 9-bit if PCE is set).

LINFLEX[nbLINFlex]->UARTCR.B.TxEn = 1;
LINFLEX[nbLINFlex]->UARTCR.B.RxEn = 1;


LINFLEX_InitRxBuffer(nbLINFlex,1);

LINFLEX[nbLINFlex]->UARTSR.B.DRFRFE = 1; // clear DRF flag (Data Reception Complete Flag)
LINFLEX[nbLINFlex]->UARTSR.B.DTFTFF = 1; // clear DTF flag (Data Transmission Complete Flag)
LINFLEX[nbLINFlex]->LINCR1.B.INIT = 0; // enter normal mode

Is there any solution to solve this. 

0 Kudos

1,177 Views
hbw
Contributor I

You can try functions from this demo,which I find from S32 Design Studio for Power Architecture

/*
* linflexd_uart.c
*
* Created on: Mar 2, 2016
* Author: B55457
*/

#include "linflexd_uart.h"

unsigned char UARTFirstTransmitFlag_0;
unsigned char UARTFirstTransmitFlag_1;
/*****************************************************************************/
/*
** Baud Rate = LINCLK / (16 x LFDIV)
** LINCLK = BR x (16 x LFDIV)
** LINCLK / (BR x 16) = LFDIV
**
** LFDIV = Mantissa.Fraction.
** Mantissa = LINIBRR
** Fraction = LINFBRR / 16
**
** Baud Rate = LINCLK / (16 x LINIBRR.(LINFBRR / 16))
** LINIBRR.(LINFBRR / 16) = LINCLK / (BR x 16)
** LINIBRR = Mantissa[LINCLK / (BR x 16)]
** Remainder = LINFBRR / 16
** LINFBRR = Remainder * 16
** The Remainder is < 1, So how does the Remainder work during a divide?
** May be best to use a table?
**
** For Refernce & Quick Tests
** LINFLEX_x.LINIBRR.R = 416; // 9600 at 64MHz
** LINFLEX_x.LINFBRR.R = 11;
**
** LINFLEX_x.LINIBRR.R = 781; // 9600 at 120MHz
** LINFLEX_x.LINFBRR.R = 4;
*/
/*****************************************************************************/

void initLINFlexD_1 ( unsigned int MegaHertz, unsigned int BaudRate ) {
unsigned int Fraction;
unsigned int Integer;

LINFlexD_1.LINCR1.B.INIT = 1; /* Enter Initialization Mode */
LINFlexD_1.LINCR1.B.SLEEP = 0; /* Exit Sleep Mode */
LINFlexD_1.UARTCR.B.UART = 1; /* UART Enable- Req'd before UART config.*/
LINFlexD_1.UARTCR.R = 0x0033; /* UART Ena, 1 byte tx, no parity, 8 data*/
LINFlexD_1.UARTSR.B.SZF = 1; /* CHANGE THIS LINE Clear the Zero status bit */
LINFlexD_1.UARTSR.B.DRFRFE = 1; /* CHANGE THIS LINE Clear DRFRFE flag - W1C */

BaudRate = (MegaHertz * 1000000) / BaudRate;
Integer = BaudRate / 16;
Fraction = BaudRate - (Integer * 16);

LINFlexD_1.LINIBRR.R = Integer;
LINFlexD_1.LINFBRR.R = Fraction;

LINFlexD_1.LINCR1.B.INIT = 0; /* Exit Initialization Mode */

UARTFirstTransmitFlag_1 = 1; /* Indicate no Tx has taken place yet */

/* Configure LINFlexD_1 TxD Pin. */
SIUL2.MSCR[PD9].B.SSS = 2; //Pad PD9: Set to LINFlex_1 TxD. Must choose this option because F14 leads to LIN PHY of motherboard
SIUL2.MSCR[PD9].B.OBE = 1; //Enable output buffer
SIUL2.MSCR[PD9].B.SRC = 3; //Full drive-strength without slew rate control

/* Configure LINFlexD_1 RxD Pin. */
SIUL2.MSCR[PD12].B.IBE = 1; //Pad PD12: Enable input buffer
SIUL2.IMCR[166].B.SSS = 0b0010; //Connect LINFlexD_2 signal to PD12
}
/*****************************************************************************/

char message_1[] = {"\n\rThis is the DEVKIT-MPC5744P UART test. If you see this in your PC terminal, test was successful.\n\r"};

void testLINFlexD_1( void ) { /* Display message to terminal */

int i, size;
size = sizeof(message_1);
/* Send to LINFlex_1. */
for (i = 0; i < size; i++) {
txLINFlexD_1(message_1[i]); //Send from LINFlex_1
}
}
/*****************************************************************************/

unsigned char rxLINFlexD_1() {
while (LINFlexD_1.UARTSR.B.DRFRFE == 0); /* Wait for dta reception complete*/
LINFlexD_1.UARTSR.R &= UART_DRFRFE; /* Clear data receptoin flag W1C */
return( LINFlexD_1.BDRM.B.DATA4 ); /* Read byte of Data */
}
/*****************************************************************************/

void txLINFlexD_1( unsigned char Data ) {
if( UARTFirstTransmitFlag_1 ) { /* 1st byte transmit after init: */
UARTFirstTransmitFlag_1 = 0; /* Clear variable */
}
else { /* Normal tranmit (not 1st time): */
while (LINFlexD_1.UARTSR.B.DTFTFF == 0); /* Wait for data trans complete*/
LINFlexD_1.UARTSR.R &= UART_DTFTFF; /* Clear DTFTFF flag - W1C */
}
LINFlexD_1.BDRL.B.DATA0 = Data; /* Transmit 8 bits Data */
}
/*****************************************************************************/

unsigned char checkLINFlexD_1() { /* Optional utility for status check */
return( LINFlexD_1.UARTSR.B.DRFRFE ); /* Return Receive Buffer Status */
}
/*****************************************************************************/

void echoLINFlexD_1() { /* Optional utility to echo char. */
txLINFlexD_1( rxLINFlexD_1() );
}
/*****************************************************************************/

void initLINFlexD_0 ( unsigned int MegaHertz, unsigned int BaudRate ) {
unsigned int Fraction;
unsigned int Integer;

LINFlexD_0.LINCR1.B.INIT = 1; /* Enter Initialization Mode */
LINFlexD_0.LINCR1.B.SLEEP = 0; /* Exit Sleep Mode */
LINFlexD_0.UARTCR.B.UART = 1; /* UART Enable- Req'd before UART config.*/
LINFlexD_0.UARTCR.R = 0x0033; /* UART Ena, 1 byte tx, no parity, 8 data*/
LINFlexD_0.UARTSR.B.SZF = 1; /* CHANGE THIS LINE Clear the Zero status bit */
LINFlexD_0.UARTSR.B.DRFRFE = 1; /* CHANGE THIS LINE Clear DRFRFE flag - W1C */

BaudRate = (MegaHertz * 1000000) / BaudRate;
Integer = BaudRate / 16;
Fraction = BaudRate - (Integer * 16);

LINFlexD_0.LINIBRR.R = Integer;
LINFlexD_0.LINFBRR.R = Fraction;

LINFlexD_0.LINCR1.B.INIT = 0; /* Exit Initialization Mode */

UARTFirstTransmitFlag_0 = 1; /* Indicate no Tx has taken place yet */

/* Configure LINFlexD_0 TxD Pin. */
SIUL2.MSCR[PB2].B.SSS = 0b0001; //Pad PF14: Set to LINFlex_0 TxD. Must choose this option because F14 leads to LIN PHY of motherboard
SIUL2.MSCR[PB2].B.OBE = 1; //Enable output buffer
SIUL2.MSCR[PB2].B.SRC = 3; //Full drive-strength without slew rate control

/* Configure LINFlexD_0 RxD Pin. */
SIUL2.MSCR[PB3].B.IBE = 1; //Pad PF15: Enable input buffer
SIUL2.IMCR[165].B.SSS = 0b0001; //Connect LINFlexD_0 signal to PTB3
}
/*****************************************************************************/

//char message[] = "Welcome to MPC5748G! ";

char message_0[] = {"Hello"};

void testLINFlexD_0( void ) { /* Display message to terminal */
int i, size, j;
uint8_t result[sizeof(message_0)] = {0};

size = sizeof(message_0);
/* Send to LINFlex_1. */
for (i = 0; i < size; i++) {
txLINFlexD_0(message_0[i]); //Send from LINFlex_0
result[i] = rxLINFlexD_1(); //Get the character from LINFlex_0

if(result[i] == message_0[i]){ //Flash PA0 5 times if result is the same as the sent character
SIUL2.GPDO[PA0].B.PDO = 0;
for(j = 0; j < 5; j++){
int counter = 0;
SIUL2.GPDO[PA0].B.PDO ^= 1; //Toggle LED
while(counter < 50000){ //Wait
counter++; //increment counter
}
counter=0;
}
}
}
}
/*****************************************************************************/

unsigned char rxLINFlexD_0() {
while (LINFlexD_0.UARTSR.B.DRFRFE == 0); /* Wait for dta reception complete*/
LINFlexD_0.UARTSR.R &= UART_DRFRFE; /* Clear data receptoin flag W1C */
return( LINFlexD_0.BDRM.B.DATA4 ); /* Read byte of Data */
}
/*****************************************************************************/

void txLINFlexD_0( unsigned char Data ) {
if( UARTFirstTransmitFlag_0 ) { /* 1st byte transmit after init: */
UARTFirstTransmitFlag_0 = 0; /* Clear variable */
}
else { /* Normal tranmit (not 1st time): */
while (LINFlexD_0.UARTSR.B.DTFTFF == 0); /* Wait for data trans complete*/
LINFlexD_0.UARTSR.R &= UART_DTFTFF; /* Clear DTFTFF flag - W1C */
}
LINFlexD_0.BDRL.B.DATA0 = Data; /* Transmit 8 bits Data */
}
/*****************************************************************************/

unsigned char checkLINFlexD_0() { /* Optional utility for status check */
return( LINFlexD_0.UARTSR.B.DRFRFE ); /* Return Receive Buffer Status */
}
/*****************************************************************************/

void echoLINFlexD_0() { /* Optional utility to echo char. */
txLINFlexD_0( rxLINFlexD_0() );
}
/*****************************************************************************/

0 Kudos

1,177 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can refer to this example https://community.nxp.com/docs/DOC-104681 

BR, Petr

0 Kudos

1,177 Views
hbw
Contributor I

Hi,

      Petr,thank you for your explain.I have found the detail about the Clock configuration for the LINFlex Module.It is from the 347th of the MPC5744PRM.Therefore my problem has been solved.That's all.

      Best Wishes.

W,Hb

0 Kudos