Can3 of MPC5606B Rx electrical level is not normal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can3 of MPC5606B Rx electrical level is not normal

827 Views
iswanghe
Contributor II

Hi, I am Wang He. Now I am Using MPC5606B to manage 6ch CAN bus. Can3 Rx electrical level is not normal while the other 5ch CAN bus are normal.

 

Can3 Rx wave form is like this:

Low level is 2V,  not 0V, while the other 5ch CAN bus Rx is 0V.

152731_152731.bmp1.bmp

Schematic is like this:(the 6ch CAN bus are same)

 

152745_152745.bmp3.bmp

The configuration of CAN3 is different from the other 5ch CAN bus is:

SIU.PCR[36].R = 0x0101;

SIU.PCR[37].R = 0x0A01;

 

For eaxmple, CAN4's configuration is like this:

SIU.PCR[94].R = 0x0601;

SIU.PCR[95].R = 0x0101;

 

I am looking forward to your guide. THANK You very much!

Labels (1)
Tags (1)
0 Kudos
3 Replies

655 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Try to swap 2 digital isolators to check if the issue is really due to PC[4] pin or external HW. What is the signal on transceiver's RXD3 output?

Also be sure there is nothing else connected to the PC[4] pin and finally check the PCR[36] is not modified from your setting.

BR, Petr

0 Kudos

655 Views
iswanghe
Contributor II

Hi,

Thank you for your reply.

Digital isolator of CAN3 is normal(I have swaped ). The waveform on Transceiver's RXD3 and isolator's RXD are nomal also.

I am very curious. What problems can cause the waveform.(Low level is 2V,  not 0V)

0 Kudos

655 Views
PetrS
NXP TechSupport
NXP TechSupport

I did a quick test with CAN_3 module on TRK-MPC5606B and have no issue. RX pin (PC4) has normal levels.

Try to use different pin for CAN3RX, PE[9] or PF[9]) if those are not used.

BR, Petr

0 Kudos