Dear NXP engineer:
I want to use the portD as a external interrupt,as you know,The SIUL only supports 32 external interrupts,As shown in the figure below
So,I have two question:
1.Can be used as external interrupt port D?
2.If it can’t,Want to use the port D as an external interrupt source is there any way can replace?
Please give me your valuable answer!
Thanks!
Hi, only those pins having EIRQ functionality can be used. Port D does not have such one.