Can I modify the boot header information?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I modify the boot header information?

ソリューションへジャンプ
531件の閲覧回数
kimdukyu
Contributor II

Hi. NXP Community.

 

We are developing a program based on SDK 3.0.3 in S32DS Studio (IDE).

I want to program the data of the Configuration Bits (0Ch) address of the boot header. Please support me on which file to refer to to manipulate the Configuration Bits (0Ch) address.

Thank you very much.

0 件の賞賛
返信
1 解決策
516件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you tell me which micro you are using and which version of S32DS?

Bootheader can be modified simply via defines:

petervlna_0-1664784234702.png

Best regards,

Peter

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
517件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you tell me which micro you are using and which version of S32DS?

Bootheader can be modified simply via defines:

petervlna_0-1664784234702.png

Best regards,

Peter

 

0 件の賞賛
返信