Can I modify the boot header information?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I modify the boot header information?

Jump to solution
469 Views
kimdukyu
Contributor II

Hi. NXP Community.

 

We are developing a program based on SDK 3.0.3 in S32DS Studio (IDE).

I want to program the data of the Configuration Bits (0Ch) address of the boot header. Please support me on which file to refer to to manipulate the Configuration Bits (0Ch) address.

Thank you very much.

0 Kudos
Reply
1 Solution
454 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you tell me which micro you are using and which version of S32DS?

Bootheader can be modified simply via defines:

petervlna_0-1664784234702.png

Best regards,

Peter

 

View solution in original post

0 Kudos
Reply
1 Reply
455 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you tell me which micro you are using and which version of S32DS?

Bootheader can be modified simply via defines:

petervlna_0-1664784234702.png

Best regards,

Peter

 

0 Kudos
Reply