CAN FD support in MPC560XX  Family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN FD support in MPC560XX  Family

4,162件の閲覧回数
dipakpatil
Contributor II

Hello All,

Is there any other micro of family MPC560xx which supports CAN FD?

ラベル(1)
8 返答(返信)

2,580件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

CAN-FD is not present on any MPC56xx device, it is available with certain MPC57xx device only.

2,252件の閲覧回数
pederrogo
Contributor III

Assume CAN-FD is not supported by any MPC55xx device either, correct?
We are for example using MPC5517....

0 件の賞賛
返信

2,580件の閲覧回数
dipakpatil
Contributor II

Hello David,

David Tosenovjan

Can you please tell us the exact part details of this micro (MPC570x with e200z0 core) ? If possible share the link for datasheet....

0 件の賞賛
返信

2,580件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

MPC5777M

MPC5777C

MPC5748G

MPC5746R

MPC5775K

None uses e200z0, they use z7, z4 and z2 cores.

2,580件の閲覧回数
dipakpatil
Contributor II

We are currently using the micro SPC5602BK0MLL4, 24k RAM 256K flash and we are looking new micro with below requirements,

Memory Requirements :

     ROM 1 MB

     RAM ≥ 64 KB

     Data Flash ≥ 64 KB

Other Major Peripherals :

     CANFD capable

     2 LIN channels

     2 CAN channel

     7 analog I/P ports

please suggest lowest package possible micros with minimum changes for porting current SW to new micro.

0 件の賞賛
返信

2,580件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

As there is lot of options, firstly I would recommend to see following selector guide:

http://www.freescale.com/files/microcontrollers/doc/roadmap/BRAUTOPRDCTMAP.pdf

2,580件の閲覧回数
dipakpatil
Contributor II

Hello davidtosenovjan

Do you have any document stated the difference between these cores ?

0 件の賞賛
返信

2,580件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have shared old presentation that compares and describes e200 cores:

e200 Core Training

Regarding MPC57xx there is also overview document that could be useful:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN4802.pdf

http://www.nxp.com/webapp/Download?colCode=DWF14-AMF-AUT-T0345