Hello everyone,
I would like to calculate MISR signature using MISR_C55.exe application. However, I could not understand how exactly I can use this app for my purpose. Could you give me feedback me about that? Btw, My mcu is MPC5777C
Sincerely.
解決済! 解決策の投稿を見る。
Hi Berat,
I wrote an example for MPC5744P:
This could move you forward.
See the readme.txt of the tool (the path is c:\Program Files (x86)\Freescale\Standard Software Driver v1.1.0\MPC57xx\Tool\MISR_gen\readme.txt) and then see misr.bat in my example.
Regards,
Lukas
Hi Berat,
I wrote an example for MPC5744P:
This could move you forward.
See the readme.txt of the tool (the path is c:\Program Files (x86)\Freescale\Standard Software Driver v1.1.0\MPC57xx\Tool\MISR_gen\readme.txt) and then see misr.bat in my example.
Regards,
Lukas
Dear @lukaszadrapa
Thank you for your kind response.
What could be the reason warning in the photo attached below? Could you give me feedback?
Sincerely.
Hi Berat,
you use MPC5777C, so you need to use this file:
c:\Program Files (x86)\Freescale\Standard Software Driver v1.1.0\MPC57xx\Tool\MISR_gen\startAddr_example\MPC5777C_startAddress.txt
And notice that this file must be either in the same folder as MISR_55.exe or use whole path in the command parameter.
Regards,
Lukas
Hello Lukas,
When I run the misr.bat from the provided example (using MPC5777C_startAddress.txt from startAddr_example directory) I get the following error:
Do you know what could be the issue?
I'm using MPC5777C.
Best regards,
Valentin
Issue is resolved when C55FMC_MCRE register value is used as -m parameter value.