Hello , I have some problems about the ADC configuration of the MPC5744P.
The configuration steps are bellow:
1. SIUL2_MSCR(PE7) = SIUL2_MSCR_APC;
2. NCMR0.B.CH6 =1u;
3. ADC0 Module Calibration;
4. ADC0 Module Init;
for(;;){
read specified channel value.
}
Then the program run.
When the PE7 is hang in the air, the pin measured with 100mv voltage . Was it right ?
Hi,
yes, if you measure floating pin you can get nonzero value as conversion result.
BR, Petr