The queries on MPC5676R ADC are explained in detail in the attachment. Please look into them and reply as soon as possible.
Thank you
Hi,
ETRIGx are external trigger signals to the eQADC module. Still it represents internal signals which source can be selected by the SIU.ISEL[4-7] registers. See chapter 3.2.1.18 and Table 3-27 to Table 3-38 of the device Reference manual.
For example Table 3-27. eQADC_A Command FIFO 0 Trigger Sources
So many PIT, eTPU and eMIOS channels can be selected and also you can locate 2 external signals called “eTRIG0 pin” and “eTRIG1 pin”. These are available on pads AF23 and AD6(AA8)
BR, Petr