ADC Accuracy

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC Accuracy

903 次查看
kavithakakarla
Contributor II

Hi,

We are using NXP MPC5746C MicroController for one of our projects.

We have used external Multiplexers (PartNumber: 74HC4051PW) to connect to ADC_0. 

Below are the configurations I used for ADC_0:

ADC Bus clock(FS80) is set to 80MHz using a system clock of 160 MHz.

ADC Clock - 40MHz ( ADC_0.MCR.B.ADCLKSEL = 0 - Half of the bus clock)

Sample Time - 0.6 microseconds (ADC_0.CTR2.B.INPSAMP = 24)

Decode Signal Delay - 2.5 micro seconds (ADC_0.DSDR.B.DSD = 100)

One shot mode and Normal Conversion is enabled for all the external Channels(64 to 95) of ADC_0.

With this configuration I applied a voltage of 0.337V to one of the external channels and expected to observe the ADC Count as 69. But I have observed the ADC Count as 77.

If I change the decode signal delay (ADC_0.DSDR.B.DSD) to 4000 (which is approximately 50microseconds), only then I am receiving the ADC Count as 69.

But increasing the DSD shall increase the total conversion time which may make our system  slow.

Please suggest if we should use a delay of 4000 values in DSD register to get the accurate ADC results or is there any other solution to increase the ADC Accuracy.

Note:

Using this DSD delay, to convert 32 external channels (Decode Signal delay of 50*8 = 400 microseconds + sampling time of ~1*8 = 8 => Results in total of ~410microseconds)

Please correct me if above calculation is wrong

Thanks

0 项奖励
回复
1 回复

775 次查看
jamesmurray
Contributor V

I face a similar problem. There needs to be more detailed information about this in the manuals. I'm going to post a new topic on this subject.

James

0 项奖励
回复