00000000: se_illegal or 01002bc8: e_b 0x1002bc8 <uSDHC_DriverIRQHandler> error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

00000000: se_illegal or 01002bc8: e_b 0x1002bc8 <uSDHC_DriverIRQHandler> error

935 次查看
turkmani_11
Contributor III

hi , im trying to solve this problem, i get it when the program comes to the exit the end of this function:

turkmani_11_0-1666617309716.png

i get this :

turkmani_11_1-1666617461651.png

or i get this:

turkmani_11_2-1666617584122.png

 

can you please give me possible solutions

 

 

0 项奖励
回复
5 回复数

925 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

which command / asm instruction is causing this exactly?

Regards,

Lukas

0 项奖励
回复

923 次查看
turkmani_11
Contributor III

i have this function:

turkmani_11_0-1666871433703.png

it passes all arguments but cant get out of it, also when i erase this line  DSPI_MasterTransferBlocking(DSPI0_INSTANCE, test_buf , master_receive, sample_size, TIMEOUT);

it doesnt give me the error so i guess its this line where i send  a message through dspi

0 项奖励
回复

919 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

This does not help much. It would require some extensive debugging. I'm not able to say what's wrong from provided information.

Regards,

Lukas

0 项奖励
回复

915 次查看
turkmani_11
Contributor III

With what information shall i provide you?

0 项奖励
回复

899 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

I would need to know which instruction/command is causing the fault exactly (at the level of instructions, not functions) with some context like content of core registers etc.

Second option is to provide very simple test project to be able to reproduce the issue on my side (it should be possible to run it on EVB).

Regards,

Lukas

0 项奖励
回复