Example MPC5748G PretendedNetworkingCAN S32DS_1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5748G PretendedNetworkingCAN S32DS_1.0

Example MPC5748G PretendedNetworkingCAN S32DS_1.0

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed

* frequency

*

*

* Mode transition to LPU_STOP is executed. CAN_0 is configured to wake up from

*  LPU_STOP to LPU_RUN using message with standard IDE = 0 as a wake up

*  preselected matching criteria. After wake up from LPU_STOP, user

*  LED1 is blinking.

 

*

* Modified files: mem.ld, sections.ld, startup.s, added file z2_restart.s

*

*

* ------------------------------------------------------------------------------

* Test HW:         MPC5748G-324DS, MPC574xG Motherboard

* MCU:             PPC5748GMMN6A 1N81M

* Fsys:            PLL0 160MHz

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Target:          internal_FLASH (debug mode, release mode)

* EVB connection:  Default

*

*

*

********************************************************************************

ラベル(1)
添付
コメント

Hi,

Can I use U-multilink to test this code?When I use this tool, I can not debug properly.

pastedImage_1.png

評価なし
バージョン履歴
最終更新日:
‎03-24-2016 05:42 AM
更新者: