Example MPC5668G PinToggleStationery CW210

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5668G PinToggleStationery CW210

Example MPC5668G PinToggleStationery CW210

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt, starts second core

* initializes and display notice via UART terminal and then terminals ECHO.

*

*

* Test HW:              MPC5688EVB

* MCU:                   SPC5668GMMG 0N61C

* Terminal:              19200-8-no parity-1 stop bit-no flow control on eSCI_A

* Fsys:                   116 MHz

* Debugger:             Lauterbach Trace32

*                             PeMicro USB-ML-PPCNEXUS

* Target:                  RAM, internal_FLASH

* EVB connection:   User LED 4 connected to pin P28-10

*

*

标签 (1)
附件
无评分
版本历史
最后更新:
‎12-29-2015 03:46 AM
更新人: