Example MPC5606S-DEMO LM75B+TFT CW210

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5606S-DEMO LM75B+TFT CW210

Example MPC5606S-DEMO LM75B+TFT CW210

Detailed Description:

Demo application performs I2C communication with externally connected

temperature sensor LM75B. Obtained values and processed and displayed on

MPC5606S-DEMO-V2 board’s TFT panel.

Application uses standard Graphics Libraries for MPC5606S for simple graphic

output that is managed in mc_base.c module only.

I2C communication is managed with using of own two layer driver where

low-level driver consisting of I2C_0.c and I2C_0.h - these can be used for

any device connected to I2C_0 module.

Middle-level driver layer consist of I2C_LM75B.c and I2C_LM75B.h and

it is specific to LM75B device.

------------------------------------------------------------------------------

Test HW:            MPC5606S-DEMO-V2 + LM75BD

MCU:             PPC5606SEF OMLU 0M25V DD68391 XOTAC1003

Fsys:            64MHz

Debugger:        Lauterbach Trace32

Target:          internal_FLASH

Terminal:        none

EVB connection:

152532_152532.png

 

For complete project you may see following link:

Demo application MPC5606S-DEMO + LM75B + HIH-5030 + PCA8565 + GUI

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎05-27-2016 06:14 AM
更新者: