Hello,
When I configured as standart ID's, I received CAN messages.
But When I set CAN ID as extended, I do not received CAN messages.
Do I miss a any configuration that I need?
Here is CAN2_init function:
void CAN2_Init(void)
{
GPIO_PinInit(GPIO10, 1U, &pinConfig); // CAN2 STANDBY PIN INIT
GPIO_PinInit(GPIO4, 6U, &pinConfig); // CAN2 ENABLE PIN INIT
GPIO_PinWrite(GPIO10, 1U, 1U); // CAN2 STANDBY HIGH
GPIO_PinWrite(GPIO4, 6U, 1U); // CAN2 ENABLE HIGH
flexcan_config_t flexcanConfig;
flexcan_rx_mb_config_t mbConfig;
flexcan_rx_mb_config_t mbConfig1;
flexcan_rx_mb_config_t mbConfig2;
flexcan_rx_mb_config_t mbConfig3;
clock_root_config_t rootCfg = {0};
rootCfg.mux = FLEXCAN_CLOCK_SOURCE_SELECT;
rootCfg.div = FLEXCAN_CLOCK_SOURCE_DIVIDER;
CLOCK_SetRootClock(kCLOCK_Root_Can2, &rootCfg);
FLEXCAN_GetDefaultConfig(&flexcanConfig);
flexcan_timing_config_t timing_config;
memset(&timing_config, 0, sizeof(flexcan_timing_config_t));
if (FLEXCAN_CalculateImprovedTimingValues(CAN2, flexcanConfig.bitRate, EXAMPLE_CAN_CLK_FREQ, &timing_config))
{
/* Update the improved timing configuration*/
memcpy(&(flexcanConfig.timingConfig), &timing_config, sizeof(flexcan_timing_config_t));
}
else
{
// LOG_INFO("No found Improved Timing Configuration. Just used default configuration\r\n\r\n");
}
FLEXCAN_Init(CAN2, &flexcanConfig, EXAMPLE_CAN_CLK_FREQ);
/* Create FlexCAN handle structure and set call back function. */
FLEXCAN_TransferCreateHandle(CAN2, &flexcanHandle, flexcan_callback, NULL);
/* Set Rx Masking mechanism. */
FLEXCAN_SetRxMbGlobalMask(CAN2, FLEXCAN_RX_MB_EXT_MASK(0x1FFFFFFF, 0, 0)); //0x18DAFFF9 0x625
/* Setup Rx Message Buffer. */
mbConfig3.format = kFLEXCAN_FrameFormatExtend;
mbConfig3.type = kFLEXCAN_FrameTypeData;
mbConfig3.id = FLEXCAN_ID_EXT(0x18DAFFF9);
FLEXCAN_SetRxMbConfig(CAN2, RX_MESSAGE_BUFFER_NUM3, &mbConfig3, true);
/* Setup Tx Message Buffer. */
FLEXCAN_SetTxMbConfig(CAN2, TX_MESSAGE_BUFFER_NUM3, true);
/* Start receive data through Rx Message Buffer. */
rxXfer.mbIdx = (uint8_t)RX_MESSAGE_BUFFER_NUM;
rxXfer.frame = &rxFrame1;
(void)FLEXCAN_TransferReceiveNonBlocking(CAN2, &flexcanHandle, &rxXfer);
rxXfer1.mbIdx = (uint8_t)RX_MESSAGE_BUFFER_NUM1;
rxXfer1.frame = &rxFrame2;
(void)FLEXCAN_TransferReceiveNonBlocking(CAN2, &flexcanHandle, &rxXfer1);
rxXfer2.mbIdx = (uint8_t)RX_MESSAGE_BUFFER_NUM2;
rxXfer2.frame = &rxFrame3;
(void)FLEXCAN_TransferReceiveNonBlocking(CAN2, &flexcanHandle, &rxXfer2);
rxXfer3.mbIdx = (uint8_t)RX_MESSAGE_BUFFER_NUM3;
rxXfer3.frame = &rxFrame4;
(void)FLEXCAN_TransferReceiveNonBlocking(CAN2, &flexcanHandle, &rxXfer3);
CAN2_BSI4_frame.length = (8U);
CAN2_BSI4_frame.format = kFLEXCAN_FrameFormatExtend;
CAN2_BSI4_frame.type = kFLEXCAN_FrameTypeData;
/* Start receive data through Tx Message Buffer. */
txXfer3.mbIdx = (uint8_t)TX_MESSAGE_BUFFER_NUM3;
txXfer3.frame = &CAN2_BSI4_frame;
}
Hi,
Can you tell us the part number you are using? the IP of CAN module is different for different family.
BR
XiangJun Rong
Hi,
The customer use imxRT1170 Processor
BR
XiangJun Rong
Hi,
Thank you so much for your interest in our products and for using our community.
There are CAN examples in the SDK, but they are configured for standard messages. An apology for the inconvenience.
Hope it helps you.
Have a nice day!