The open source hardware community is please to offer ECAD schematic symbols for the new MCX A153 and MCX N947 microcontrollers.
![Eli_H_0-1707615293073.png Eli_H_0-1707615293073.png](https://community.nxp.com/t5/image/serverpage/image-id/262767iB349BD92D946DB0D/image-size/medium?v=v2&px=400)
The MCX A153 schematic library has the QFP32, QFN48 and LQFP64 variants.
The MCX N947 schematic library has the BGA184 and LQFP100 variants.
The symbols were generated using data from the MCUXpresso Pin Config tool to ensure accuracy. The pin names include all pin mux options to make it easy to see all available peripheral functions and further simplify the symbol for your own design purpose
The symbol data is provided in the open source KiCad V7 format and is attached to this post. The symbols can be imported into commercial tools such as Altium Designer.
Enjoy!