ECAD Schematic Symbols for MCX A153 and MCX N947

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECAD Schematic Symbols for MCX A153 and MCX N947

ECAD Schematic Symbols for MCX A153 and MCX N947

The open source hardware community is please to offer ECAD schematic symbols for the new MCX A153 and MCX N947 microcontrollers.  

 Eli_H_0-1707615293073.png

The MCX A153 schematic library has the QFP32, QFN48 and LQFP64 variants.

The MCX N947 schematic library has the BGA184 and LQFP100 variants.

The symbols were generated using data from the MCUXpresso Pin Config tool to ensure accuracy. The pin names include all pin mux options to make it easy to see all available peripheral functions and further simplify the symbol for your own design purpose

The symbol data is provided in the open source KiCad V7 format and is attached to this post. The symbols can be imported into commercial tools such as Altium Designer.

Enjoy!

 

Labels (2)
Attachments
No ratings
Version history
Last update:
‎02-10-2024 06:37 PM
Updated by: