I change 0x20000000 to 0x20200000 and 0x20200000 to 0x20000000
1061 with freertos in "Low Power Idle mode",can't use gpio to wakeup
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd like to know what modification you did in addition above change, further, did you test in debug mode?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Thanks for your reply.
Actually, I'm not sure the root cause, however, I think you'd better modify the below two options besides your previous modification.
Furthermore, the issue may be related to the on/off option of the PDRAM1.
Last, I'm curious why you run the code in the RAM to test low power mode.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------