fsl_enet for i.MX RT106x not able to handle ENET2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fsl_enet for i.MX RT106x not able to handle ENET2

3,732件の閲覧回数
dirkcastelijns
Contributor I

The fsl_enet drivers in the SDK for i.MX RT106x contain some array of data structures based on the number of ENET peripherals available. There is a mismatch in number of array elements which causes a HardFault when using ENET2.

Looking at fsl_enet.c, we see several arrays being declared:

/*! @brief Pointers to enet handles for each instance. */
static enet_handle_t *s_ENETHandle[FSL_FEATURE_SOC_ENET_COUNT] = {NULL};


/*! @brief Pointers to enet clocks for each instance. */
#if !(defined(FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL) && FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL)
const clock_ip_name_t s_enetClock[] = ENET_CLOCKS;
#endif /* FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL */

/*! @brief Pointers to enet transmit IRQ number for each instance. */
static const IRQn_Type s_enetTxIrqId[] = ENET_Transmit_IRQS;
/*! @brief Pointers to enet receive IRQ number for each instance. */
static const IRQn_Type s_enetRxIrqId[] = ENET_Receive_IRQS;
#if defined(ENET_ENHANCEDBUFFERDESCRIPTOR_MODE) && ENET_ENHANCEDBUFFERDESCRIPTOR_MODE
/*! @brief Pointers to enet timestamp IRQ number for each instance. */
static const IRQn_Type s_enetTsIrqId[] = ENET_1588_Timer_IRQS;
#endif /* ENET_ENHANCEDBUFFERDESCRIPTOR_MODE */
/*! @brief Pointers to enet error IRQ number for each instance. */
static const IRQn_Type s_enetErrIrqId[] = ENET_Error_IRQS;

/*! @brief Pointers to enet bases for each instance. */
static ENET_Type *const s_enetBases[] = ENET_BASE_PTRS;

The s_ENETHandle[] array size is determined by FSL_FEATURE_SOC_ENET_COUNT defined in MIMXRT1062_features.h:

/* @brief ENET availability on the SoC. */
#define FSL_FEATURE_SOC_ENET_COUNT (2)

All the other array sizes are determine by macro's in MIMXRT1062.h:

/** Array initializer of ENET peripheral base addresses */
#define ENET_BASE_ADDRS { ENET_BASE, 0u, ENET2_BASE }
/** Array initializer of ENET peripheral base pointers */
#define ENET_BASE_PTRS { ENET, (ENET_Type *)0u, ENET2 }
/** Interrupt vectors for the ENET peripheral type */
#define ENET_Transmit_IRQS { ENET_IRQn, NotAvail_IRQn, ENET2_IRQn }
#define ENET_Receive_IRQS { ENET_IRQn, NotAvail_IRQn, ENET2_IRQn }
#define ENET_Error_IRQS { ENET_IRQn, NotAvail_IRQn, ENET2_IRQn }
#define ENET_1588_Timer_IRQS { ENET_1588_Timer_IRQn, NotAvail_IRQn, ENET2_1588_Timer_IRQn }

As you can see the macro expand to 3 elements while s_ENETHandle[] has only 2 elements. For some reason they left a gap between ENET and ENET2.  

At several places in fsl_enet.c the function ENET_GetInstance(base) is used to determine the index for one of the arrays above. Because this function iterates through s_enetBases[], the returned index can be 0 to 2 (because there are three elements).  All arrays can be accesses this way except for s_ENETHandle[] but this is done in several places in fsl_enet.c. For instance in ENET_SetHandler():

static void ENET_SetHandler(ENET_Type *base,
      enet_handle_t *handle,
      const enet_config_t *config,
      const enet_buffer_config_t *bufferConfig)
{
   uint8_t count;
   uint32_t instance = ENET_GetInstance(base);

   ...

   <removed part for clarity

   ...

   /* Save the handle pointer in the global variables. */
   s_ENETHandle[instance] = handle;

   ...

As you can imagine, things can go horribly wrong this way.

For now we got things working by setting FSL_FEATURE_SOC_ENET_COUNT to 3 but this is strange because the device has only 2 ENET's.

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,356件の閲覧回数
simosilva
Contributor I

Hi everyone,
I'm dealing with same problem, need to initialize and to run two different ENET, have you found a solution to configure and then attach the two ENETs?
do the software freeRTOS/lwip and MCUXpresso SDK drivers support 2 network interfaces?
I see in configurator under the LWIP settings that only one netif can be added...

Thank you!

0 件の賞賛
返信

3,571件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Dirk:

Thank you for your feedback, I will report this to software team.

Regards

Daniel

0 件の賞賛
返信

2,872件の閲覧回数
phantomgz
Contributor III

@danielchen

I have downloaded the current "SDK_2_12_0_MIMXRT1060-EVKB", but the same issue still exists.

ENET2.png

 

After changing to this, I can active enet2.

ENET2a.png

 

Cai.

2,868件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Thanks for feedback. I will double check it.

0 件の賞賛
返信

2,848件の閲覧回数
phantomgz
Contributor III

@danielchen 

theory, there is another issue in ethernetif1_init(), if I modified the 

ENET_BASE_ADDRS and ENET_BASE_PTRS
ENET2e.png

2,859件の閲覧回数
phantomgz
Contributor III

@danielchen 

look at the calling chain from  ENET_Init() 

ENET_GetInstance(ENET2) return 1,
s_enetClock[instance] return kCLOCK_IpInvalid,
CLOCK_EnableClock() run failed to init enet2 clock,
 

ENET2b.png

ENET2c.png

ENET2d.png