Why the support to little LVGL has been downgrade to 6.1.1 when in SDK 2.8.2 was 7.0.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why the support to little LVGL has been downgrade to 6.1.1 when in SDK 2.8.2 was 7.0.0?

Jump to solution
975 Views
mperez1
Contributor II

Hello there,

I'm struggling trying to develop a graphic application with the LVGL, and for my surprise when I updated the SDK to the new version the library version has been downgraded. So now the new examples are not running in FreeRTOS and are not using the gpu hal developed for nxp (littlelvgl/lvgl/src/lv_gpu). Why this happen? Will be there any attempt in the future releases of the SDK to use the new versions?

There is any tip in order to improve the performance of this library with the hardware of the imxrt1050?

Thanks,

Miguel

 

0 Kudos
Reply
1 Solution
966 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Why this happen? Will be there any attempt in the future releases of the SDK to use the new versions?
-- Yes, it will use the updated version of little LVGL in the future release of the SDK.
2) There is any tip in order to improve the performance of this library with the hardware of the imxrt1050?
-- In my experience, it can benefit improve the code executing performance by remapping the code to the TCM area to run, especially for crucial code.
In further, the DMA engine also is able to improve the LCD performance.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
967 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Why this happen? Will be there any attempt in the future releases of the SDK to use the new versions?
-- Yes, it will use the updated version of little LVGL in the future release of the SDK.
2) There is any tip in order to improve the performance of this library with the hardware of the imxrt1050?
-- In my experience, it can benefit improve the code executing performance by remapping the code to the TCM area to run, especially for crucial code.
In further, the DMA engine also is able to improve the LCD performance.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply