I download SDK_2.5.0_MIMX8MM5xxxLZ, But it dosen't include uSDHC Driver.
And SDMMC_STACK can't be selected from SDK Dash borad.
Are there plans to release these?
Or can SDK of other board be diverted?
Best Regards,
T.Kashiwagi
解決済! 解決策の投稿を見る。
Hello, T.Kashiwagi
You are welcome! And thank you very much for your consideration. :smileyhappy:
Have a nice day!
B.R.
Fang
Hello,
The i.MX 8M Mini is quite new, and just start with production. So the SDK are not been supported fully. I am pretty sure that the SDHC driver will been added,however I did not find the concrete date for that. I will double confirm.
Hello Mr Fang, if you have an updated time for the SD driver's release or integration into SDK 2.5.0 could you please share it? I guess I should ask if it's ready right now because if it's not I'll add write my own around the lpspi driver but if it's already available that would save me development and debug time. Thanks in advance and
Best Regards
Howard
Hi Howard
I will share the information I confirmed at that time.
--
i.MX8MM's uSDHC pheripherals are smilar to i.MXRT.
I checked that the IMX8 MM uSDHC had the following registers added to the IMXRT uSDHC.
And Reset Value of VEND_SPEC2 is different.( In IMX8MM, it was 0000_0006h)
I think I can divert the i.MX RT uSDHC driver, but I have not been able to confirm the operation.
--
Best Regards,
T.Kashiwagi
Thank you T. Kashiwagi san
Howard
Hi Fang.
Thank you responding.
> The i.MX 8M Mini is quite new, and just start with production. So the SDK are not been supported fully.
> I am pretty sure that the SDHC driver will been added,however I did not find the concrete date for that.
> I will double confirm.
OK. I am waiting for an announcement.
Best Regards,
T.Kashiwagi
Hello, T.Kashiwagi
You are welcome! And thank you very much for your consideration. :smileyhappy:
Have a nice day!
B.R.
Fang