when will mcuxpresso support be available for the Kinetis SDK-2.3.1-MK22FX512Axxx12.
I am unable to drag N drop this SDK to install in MCuXpresso.
Thank you
Hope you are doing well. Which MCUXpresso version do you have? I downloaded the same SDK version and I was able to install it with no problem.
The SDK version requires MCUXpresso v10.0.x or later.
Hope this helps.
Best Regards,
Ricardo
Noel Diviney Ayrenet Pty Ltd, Unit 3,80-88 Rodeo Drive, Dandenong South, Victoria 3175, Australia. Phone +61 413 120 892 email noel@ayrenet.com or divner@hotmail.com
Hi Ricardo,
Thank you for your response.
I am using MCUXpresso V11.1.1.
There is no Dev Board for the MK22FX512AVLH12, so I had the SDK built for the device by following the instructions on the NXP Website. I am finding that this CPU seems to be the lone orphan with regards support,
How did you obtain the SDK that you used?.
Your help much appreciated.
Regards Noel.
Hi Noel,
You can download the SDK from the MCUXpresso SDK Builder.
You are right, there is no evaluation board for MK22FX512Axxx12, but there is the SDK for the processor:
This means that the SDK doesn't have SDK examples, but it includes the Drivers you can use for your project.
Hope this helps.
Best Regards,
Ricardo
Hi Ricardo.
Thank you for all the info.
I am currently learning how to use MCUXpresso with the objective of using the Config Tools
to create a custom Project for the Mk22FX512. I am progressing reasonably well.
I am requiring to be able to enter Deep Sleep Mode and the wake up as required.
Thanks again for your help.
Best Regards Noel.