USB no longer builds with MCUXpresso SDK 2.7.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB no longer builds with MCUXpresso SDK 2.7.0

920件の閲覧回数
jeffthompson
Contributor V

I upgraded from MCUXpresso SDK 2.6.2. to 2.7.0 and now usb_usrt_drv.c fails to compile because fsl_uart,h is missing and many definitions like uart_handle_t, UART_TYPE, UART_BASE_PTRS, and others along with it. Is there an updated usb_uart_drv.c?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

817件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Jeff Thompson

 

The driver for the uart is called fsl_lpuart. Also the uart.h can be found at the components folder. You can drag these files from the sdk folder to your project.

pastedImage_2.png

 

If you have more questions do not hesitate to ask me.

Best regards,

Omar

0 件の賞賛
返信

817件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Jeff Thompson

Can you help me providing me the part number of the device you are working with?

Best regards,

Omar

0 件の賞賛
返信

817件の閲覧回数
jeffthompson
Contributor V

Omar,

It’s the MIMXRT1062DVL6A.

Jeff Thompson | Senior Electrical Engineer-Firmware

+1 704 752 6513 x1394

www.invue.com

0 件の賞賛
返信