SDK for KW31Z - does it support BLE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK for KW31Z - does it support BLE?

1,258件の閲覧回数
ChrisDarrow
Contributor III

I went to the SDK builder for MCUXpresso - https://mcuxpresso.nxp.com/en/configuration-settings - and when I request KW31Z, it does not give me the option for BLE support in the middleware. But when I select the KW41Z, then it provides the option for BLE middleware.

Why isn't the BLE middleware supported on the KW31Z? The KW31Z is only supposed to support BLE, not Thread. Therefore, I would think you should be able to build a SDK for the KW31Z that supports BLE. What am I missing?


Thanks.

1 返信

1,130件の閲覧回数
Jmart
NXP Employee
NXP Employee

Chris -

I've reported this issue to the team and they are going to review the underlying metadata for the KW31Z.

Jason