SDK 2.13.0 has emWin 6.28, but no AppWizard V1.32_6.28 yet?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK 2.13.0 has emWin 6.28, but no AppWizard V1.32_6.28 yet?

Jump to solution
1,428 Views
DaPa1
Contributor III

Hello,

NXP has updated its SDK 2.13.0 (2023-01-18) to use emWin 6.28, however after 2 months there is no AppWizard 1.32_6.28 kit for download from NXP website yet.

The latest AppWizard on NXP website is the old 1.20_6.16d: https://www.nxp.com/design/software/embedded-software/nxp-emwin-libraries:EMWIN-GRAPHICS-LIBRARY?#de...

Segger's license from AppWizard states:

2.1 If you received the Software from SEGGER as a part of the licensed emWin PRO Bundle you shall make use of the Software only in strict compliance with the terms and conditions of the associated license agreement it is distributed with.

2.2 If you receive the Software from one of the SEGGER Silicon Vendor Partners together with a license for SEGGER's emWin-Software in Object code form you shall make use of the Software only in strict compliance with such license including but not limited to the restrictions as contained therein with regard to the target CPUs the  emWin-Software in Object code form may be used with.

2.3    If neither a license for the emWin PRO Bundle is granted to you by SEGGER nor a license for SEGGER's emWin-Software in Object Code form by any of the SEGGER Silicon Vendor Partners you are not authorized to use the Software

 

We need to get the AppWizard install kit legally from NXP: when will NXP make the latest AppWizard 1.32_6.28 kit available on their website?

Thank you,

Daniel

0 Kudos
1 Solution
1,321 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi DaPa1 

This case was handled and the file was sent via transweb. Please check.

Have a nice day,

Jun Zhang

View solution in original post

9 Replies
1,372 Views
DaPa1
Contributor III

Here's a confirmation that Segger imposes that we should obtain AppWizard from the MCU vendor: https://forum.segger.com/index.php/Thread/8582-emWin-License/

 

And thank you for updating https://www.nxp.com/design/software/embedded-software/nxp-emwin-libraries:EMWIN-GRAPHICS-LIBRARY?#do... with APPWIZARDTRIAL-V136A-632A-INSTALL.exe:

0-AppWizard on NXP.png

 

But unfortunately it's not what we need, because the latest SDK 2.13.0 from NXP has emWin 6.28:

1-emWin in NXP SDK.PNG


Therefore we need AppWizard 1.32 as this is the counterpart to emWin 6.28:

2-AppWizard from Segger.png


Newer emWin 6.32 has extra features and might not be compatible with 6.28 emWin lib binary:

3-emWin changes.png


Same for the newer AppWizard 1.36a which supports new objects which also might not be known by 6.28 emWin binary:

4-AppWizard changes.png

 

Can we have the correct AppWizard kit please (V132-628) or are you going to update the SDK to contain latest emWin 6.32a to match the latest AppWizard?

Thank you,

Daniel

 

0 Kudos
1,360 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

I am checking this internally.

I will keep you informed.

Best Regards

Jun Zhang

0 Kudos
1,401 Views
DaPa1
Contributor III

No, there is no AppWizard 1.32_6.28 and there was no AppWizard 1.32_6.28 on NXP.

As can be seen, Segger's licence imposes that for "emWin-Software in Object code" we must obtain the AppWizard kit from the vendor (see point 2.2 above) else we are not authorised to use new AppWizard!

Latest NXP's SDK 2.13.0 (2023-01-18) already has the new emWin 6.28, but we cannot take it in use, because counterpart AppWizard (which should be 1.32_6.28) is missing from NXP...

0 Kudos
1,407 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi DaPa1 

Thank you for reporting this.

Do you mean  AppWizard 1.32_6.28 kit was posted on NXP website before but doesn't exist recently?

Thanks.

Jun Zhang

 

0 Kudos
1,347 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @DaPa1 

AppWizard V1.32_6.28 is not avaiable on website yet. Please create a case 

https://support.nxp.com/s/?language=en_US

and comment "assign to Jennie Zhang"

I will send you with email.

Thanks,

Jun Zhang

 

0 Kudos
1,343 Views
DaPa1
Contributor III

Thank you Jun!

Just created 

  • Case Number : 00524655

 

0 Kudos
1,322 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi DaPa1 

This case was handled and the file was sent via transweb. Please check.

Have a nice day,

Jun Zhang

1,074 Views
EmbeddedTech
Contributor III

Hi @ZhangJennie,

 

I have also previously enquired about the latest version of Appwizard. I am not able to use the emWin v6.28 as the Appwizard v1.32_6.28 is not available in NXP website. How do I get that version of Appwizard?

Thanks.

0 Kudos
1,066 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech 

Please create a case 

https://support.nxp.com/s/?language=en_US

and comment "assign to Jennie Zhang"

We will check.

Thanks

Jun Zhang

0 Kudos