Hello,
I am working with the FlexSPI on a RT1060-EVK with the 2.9.3 SDK. I have a working example of the flexspi_nor_polling example that is currently able to read/write/sector erase a QSPI device on A2.
In verifying my adaptation of the example, I noticed that the erase chip wasn't working. I was able to verify that the example project has the same issue and I've found references to the default LUT being wrong in older SDKs.(Excessive-sector-erase-times-evkmimxrt1064-flexspi-nor-polling) Ironically, the erase sector is working, but not the erase chip command.
Questions:
Attached is the example project that does not erase chips.
Hello,
I just made a couple of tests on my end, and everything went fine. Function flexspi_nor_erase_chip works without problems. I used the example project of SDK v2.10.0.
Regards,
Victor